This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
It is not recommended to use the Zener diodes in parallel connection. Even products with the same product name have variations in electrical characteristics such as Zener voltage. Therefore, there is a possibility that the current will concentrate in one of the Zener diodes, resulting in characteristic deterioration or destruction.
Assume that two Zener diodes DZ1 and DZ2 with different Zener voltages shown in Fig. 2 are connected in parallel as shown in Fig. 1. Apply the voltage Vin to reverse bias the pn junction of the Zener diode. The Zener voltage of DZ1 and DZ2 is VZ at this time.
There is a difference between the currents flowing through DZ1 and DZ2 when the Zener voltage is VZ, and as shown in Fig. 2, a higher current flow through DZ2. Do not connect Zener diodes in parallel because current might concentrate only on one diode.
| Type | Zener Voltage Vz (V) | |||
|---|---|---|---|---|
| Min | Typ. | Max | Measure-ment Current Iz (mA) |
|
| CMZB12 | 10.8 | 12 | 13.2 | 10 |
Please also refer to the FAQ below.
FAQ:Is it OK to connect multiple diodes with the same part number in parallel?
For products, please refer to the following links.