This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
SiC (Silicon Carbide) is a wide-band-gap semiconductor. Compared with Si (Silicon), as shown in the table below, it is characterized by high band gap, high electric breakdown field, high saturation speed, etc.
When reverse bias is applied to the SBD of a general structure, the depletion layer expands from the metal-semiconductor interface. The image of the electric field at this time is as shown in the figure, and is the maximum at the metal-semiconductor interface. The breakdown electric field is the theoretical maximum value of the electric field and the withstand voltage is equal to the area of the triangle indicated by the width of the depletion layer and the electric field.
Since the breakdown electric field of SiC is about 10 times that of Si, SiC SBD with high withstand voltage can be formed.
Physical characteristics of Si and main wide-band-gap semiconductors
| Property | Unit | Si | 4H-SiC | 6H-SiC | 3C-SiC | GaN | GaAs | Diamond |
|---|---|---|---|---|---|---|---|---|
| Band gap | eV | 1.12 | 3.26 | 3.02 | 2.23 | 3.39 | 1.43 | 5.47 |
| Electron mobility μe | cm2/Vs | 1400 | 1000/1200 | 450/100 | 1000 | 900 | 8500 | 2200 |
| Hole mobility μh | 600 | 120 | 100 | 50 | 150 | 400 | 1600 | |
Electric breakdown field Ec |
V/cm | 3.0×105 | 2.8×106 | 3.0×106 | 1.5×106 | 3.3×106 | 4.0×105 | 1.0×107 |
| Thermal conductivity λ | W/cmK | 1.5 | 4.9 | 4.9 | 4.9 | 2.0 | 0.5 | 20 |
Saturated electron drift velocity Vsat |
cm/s | 1.0×107 | 2.2×107 | 1.9×107 | 2.7×107 | 2.7x107 | 2.0×107 | 2.7×107 |
Relative dielectric constant ε |
11.8 | 9.7/10.2 | 9.7/10.2 | 9.7 | 9.0 | 12.8 | 5.5 |