This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
This test is not a direct lightning test, but a test that models the surge voltage/current induced in the vicinity by the effects of a lightning strike. It also includes opening and closing surges due to switching in the power system (capacitor switching, power distribution system on/off, load changes, short circuits, etc.).
ESD surge specified in IEC61000-4-2 is a problem in almost all electronic equipment. However, what is modeled in IEC61000-4-5 poses problems for communication lines, power lines and control lines of industrial equipment, and inductive loads.
This is because these surges are often caused mainly by inductance.
IEC610004-5 provides models to simulate these surges so you can check if your equipment can withstand them.
There are 5 levels of classes, and the 5 levels of classes (applied voltage: 25V to 4kV) are defined according to the equipment installation location (surge control level).
We provide IEC61000-4-5 compliant devices as devices for these countermeasures.
For products, please refer to the following links.