This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Current consumption is the current that flows from BATTERY into the power supply terminal of the audio power IC and is measured using an ammeter as shown in Fig. 1. The input power can be calculated to multiply the current consumption by BATTERY voltage.
Fig. 2 shows how to measure the output power dissipation.
In case of BTL*1 amplifiers, connect a load resistor acting as an equivalent to a loudspeaker between the output terminals, and measure the AC voltage (rms) across the load resistor with an AC voltmeter.
The output power is calculated using the obtained AC voltage and load resistance value. (Output power = AC voltage ^2/Load resistance)
*: In order to calculate the total output power for a product with multiple internal amplifiers, calculate each output power channel by channel and add them up as the total output power.
*1: BTL:Bridge Tied Load
Finally, the power dissipation is calculated by the following formula.
Power dissipation Pd = Input power: Pin - Total output power : Pout(Total) = BATTERY voltage: Vbat * current consumption: Iin – output power/1ch * Number of channels N (for multiple amplifier product when each output power is same)
Note that accurate results cannot be obtained if a voltage drop occurs due to wiring resistance, etc. during measurement. To avoid it, our recommendation is to measure the voltage near the terminals of the audio power IC.
As a reference, an example of 4-channel audio power IC is shown as below.
When BATTERY is 14.4V and the output power is 1W for each channel, power dissipation is calculated as follows.
BATTERY voltage: Vbat = 14.4V
Current consumption: Iin = 0.8A (measured)
Output Power: Pout = 1W (per channel)
Number of channels: N = 4 channels
Power dissipation : Pd = (Vbat * Iin)- (Pout * N)
= (14.4 * 0.8) – (1 * 4)
= 11.52 - 4
= 7.52 [W]
This calculation shows the intersection of the dashed lines in Pd vs output power chart in Fig. 3.
The following documents also contain related information.