This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Generally, the high-frequency response shows a peak as shown in Fig. 1 if a capacitor is connected between the output and GND, and oscillation may occur in some cases. In this case, you can suppress the peak and improve the oscillation margin by inserting a resistor (about 1 to 2.2 Ω) in series with the capacitor. Note that the oscillation margin varies depending on the product. Contact our sales representative if you wish to have detailed data.
Our audio power IC has a built-in protection circuit for internal output transistors.
If capacitors are connected in series to the output line as shown in Fig. 2, phase differences may occur between the voltage and current phases of the audio power IC output; and then the built-in protection circuit may operate unintentionally by such a phase differences. As a result of that, abnormal noise or sound cutting may appear.
Please check no occurrence of these phenomena, and select appropriate components including speakers.
The following documents also contain related information.