This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The overheat monitoring solution using Thermoflagger™ and PTC thermistors is ideal for use in power supply circuitry of both consumer and industrial equipment.
Applications are widely anticipated in both consumer and industrial sectors, primarily to monitor abnormal heat generated by DC/DC converters and motor-driven MOSFETs. (Refer to Figs. 1 and 2.)
The following documents also contain related information.