This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The undervoltage lockout (UVLO) function disables output (VOUT) of a load switch IC when its input voltage (VIN) drops below the predefined threshold so that the undervoltage condition of VIN does not make the internal control circuitry unstable, causing the load switch IC to malfunction. The following table shows the ULVO characteristics of a load switch IC, which has a typical hysteresis of 0.3 V. The UVLO function is tripped to disable VOUT when VIN drops below 2.6 V typical and automatically recovers the IC operation when VIN rises back above 2.9 V typical.
To perform a parametric search of load switch ICs with an undervoltage lockout function, click:
Other load switch ICs: