This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Buffer type products and bus switch type products have different calculation methods for the operating frequency. Buffer type products can be calculated based on the propagation delay time obtained from the CR values of the load and on-resistance. On the other hand, bus switch type products can be calculated based on the load and on-resistance CR time constant.
Each calculation method is briefly described below.
For example, the TC7SPB9306 with a switch I/O capacitance (CI/O) of 14 pF. Assume a load capacitance (CL) of 30 pF and a pullup resistor (Rpu) of 1 kΩ. Then, τ is calculated as follows:
τ = (14 pF + 30 pF) × 1 kΩ
Hence, the maximum operating frequency is calculated as roughly 20 MHz
The result of this calculation should be considered merely as an estimate under the conditions shown in the datasheet.
Level shifters should be sufficiently evaluated to ensure that they work properly under the actual operating conditions because their propagation delay times change with the board capacitance and other conditions.
The following documents also contain related information.