This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The brushless motor may not work properly because of a noise on the Hall input.
As shown in Fig. 1, the IC creates an FG signal based on the zero-cross of the Hall input.
The half-period time of the FG signal is taken as the time for a 60° electrical angle, and the modulated waveform for the next 60° electrical angle period is generated.
If there is noise in the Hall signal, chattering may occur near the zero-cross, which will also cause the FG signal to chatter.
The IC will output a modulated waveform with a high frequency due to the chattering of the FG signal.
This fast modulated waveform will continue until the next Hall zero-cross, which can cause motor malfunctions and distortion in the current waveform. Please take measures such as adding a noise filter to the Hall input to cancel the noise.
The following documents also contain related information.