This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
When photocouplers are mounted in equipment as a means of "isolation" for assuring safety such as protecting the human body against an electric shock, they may be restricted by safety standards. Including standards and criteria for assuring safety, a broad range of items related to electricity have been standardized as standards. The safety standards are divided into equipment standards, which apply to end products, and component standards, which apply to individual photocouplers.
Each country has its own safety standards based on the International Electrotechnical Commission (IEC) standards. The typical standards include UL in the U.S, VDE in Germany and BSI in Britain. The UL standards in the U.S. and the VDE standards in Germany, both of which are applicable to photocouplers, have completely different definitions of test methods for measuring input-output insulation performance and of acceptance criteria.
For details, also refer to Toshiba Application Note "Safety Standards for Photocouplers", Chapters 1 to 3.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)