This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Variable capacitance diode should be selected.
A range of tuning voltage (VT) is specified for each variable-capacitance diode.
The minimum and maximum capacitances of a variable-capacitance diode are determined by its maximum and minimum tuning voltages.
We are preparing a product list (Parametric Search) with minimum and maximum capacity values, so please check here.
Parametric Search URL: https://toshiba.semicon-storage.com/list/index.php?code=param_209&lang=en
See the datasheets for the tuning voltages that provide the minimum and maximum capacitances.
When using it with an oscillator etc., attention must also be paid to the series resistance rS which determines Q (Quality Factor).
Since the above table also shows the series resistance (rS), please refer to when selecting it.