This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
It is an inverter circuit that drives a motor.
For example, a three-phase small motor has 6 power elements and 6 diodes. The power elements have transistors, FETs, IGBTs, etc.
Since the actual motor is driven by a high voltage and current, a drive circuit, which converts the PWM output of the control circuit to high voltage and large current, is required.
A pre-driver is required since a high drive current supporting around 12 volts is required to drive power elements such as FETs and IGBTs that drive the motors.
A low power motor with low voltage can be driven without a pre-driver.