4-8. Speed ​​Sequence

Speed ​​Sequence

This is an example of a sequence that changes the speed (sine-wave drive).

* Even if there is a load change on the motor, the number of rotations can be maintained by performing the above processing.

Chapter 4 Let's Try to Rotate the Motor

4-1. Configuration of Square-Wave Drive
4-2. To Start with Square-Wave Drive
4-3. To Rotate by Square-Wave Drive
4-4. Configuration of Sine-Wave Drive
4-5. To Start with Sine-Wave Drive
4-6. To Rotate by Sine-Wave Drive
4-7. To Change Speed
A new window will open