4-5. To Start with Sine-Wave Drive

To Start with Sine-Wave Drive

The brushless motor is a synchronous motor, which means that the rotation of the shaft is synchronized with the frequency of the supply current; the rotation period is exactly equal to an integral number of AC cycles.
It is not possible to start the motor using a sine-wave drive, because the stopped rotor does not follow the frequency when starting.
Therefore, when starting the motor, the acceleration operation is required by feeding back the rotor position.

  • (1) Detect the rotor position.
  • (2) Apply a sinusoidal voltage slowly to the coil according to the rotor position.
  • (3) Rotate while gradually increasing the voltage.
  • (4) Control the period of the sine-wave according to the timing of the position detection sensor.
  • (5) If the rotor rotates with a certain speed, steady operation starts to reach the target speed.

In steady operation, the speed can be maintained against load fluctuations by feeding back the target speed deviation.

*Synchronous motor may be able to start if there is no load.

Chapter 4 Let's Try to Rotate the Motor

4-1. Configuration of Square-Wave Drive
4-2. To Start with Square-Wave Drive
4-3. To Rotate by Square-Wave Drive
4-4. Configuration of Sine-Wave Drive
4-6. To Rotate by Sine-Wave Drive
4-7. To Change Speed
4-8. Speed ​​Sequence
A new window will open