1-2. Logic Circuit

Three types of basic logic element
Three types of basic logic element

Now, let's learn about the logic circuit of a microcontroller.

The logic here means that the relation between the input and output of the digital signal handled by the electronic circuit is performed according to a certain theory. The electronic circuit that performs this is called the logic circuit.
Microcontrollers consist of extremely complex logic circuits. Every logic circuit consists of a combination of three types of the basic logic element.

Chapter 1 Basics of Digital Circuits

1-1. Digital Value
1-1-1. Digital Value: Binary and Decimal
1-1-2. Digital Value: Units of Binary Data
1-1-3. Digital Value: Notation Method of Data
1-1-4. Digital Value: Conversion Method of the Data
1-2-1. Logic Circuit: AND Circuit
1-2-2. Logic Circuit: OR Circuit
1-2-3. Logic Circuit: NOT Circuit
1-2-4. Logic Circuit: Exclusive OR (XOR) Circuit
1-2-5. Logic Circuit: 3 State Buffer (1)
1-2-6. Logic Circuit: 3 State Buffer (2)
1-2-7. Logic Circuit: Application Example of Logic Circuits
1-2-8. Logic Circuit: RS flip-flop Circuit
A new window will open