This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Let's think about the relation between the binary number and the decimal number.
First, let's consider the decimal number that we use every day.
For example, if the number is 1359 (Decimal), add 1 and it will be 1360.
In this way, the decimal number, when it exceeds 9, it becomes 10, and a carry occurs.
1359 can be disassembled as shown in the formulate in the figure on the right.
The 10³, 10², 10¹, and 10º used here are called “weight”.
Now, let's look at case of the binary number.
Binary is a number consisting of 0 and 1, and when it becomes 2, a carry occurs.
For example, let's add the weight to 1110 (Binary).
In case of the binary number, the weight becomes such as 2³, 2², 2¹, 2º.
When you calculate this formula, it can convert to the decimal number.
In this case, 8+4+2+0 becomes 14.
In this way, the decimal number goes up to 1, 10, 100, and 1000 digits, but the binary number goes up to 1, 2, 4, and 8 digits.