This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
A Zener diode is a type of pn junction diode. Zener diodes are used in the breakdown region (yield region) by applying a voltage in the opposite direction to normal pn junction diodes.
Zener diode is a type of pn junction diode. Fig. 1 shows the V–I curve of the pn junction diode. Typical pn junction diodes are used with a forward bias whereas Zener diodes are used with a reverse bias as they are designed to operate in the breakdown region. There are the following two breakdown mechanisms depending on the dopant concentration of the p-type and n-type semiconductors. Since both breakdown events occur at a fixed voltage when temperature is constant, Zener diodes are also called voltage regulator diodes and constant-voltage diodes.
In practice, there are no distinct regions in which these breakdown events occur. Zener breakdown is more dominant below 6 V whereas avalanche breakdown is more dominant above 6 V.
For products, please refer to the following links.