This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
In general, power and input should be applied in the following order to satisfy the absolute maximum ratings.
If the power supply and input signals of the general-purpose logic IC are in the wrong order, it may cause malfunction, destruction, or damage to the IC or equipment, so be careful.
(1)Connect GND
(2)Connect VCC (on)
(3)Connecting Input Signals (Turning On)
Turn off the power supply in the reverse order of turning on the power supply.
ICs without an input tolerant function (such as the TC74HC/HCT series) have a protection diode on the input side as shown in Fig. 1. If the order is incorrect, an unnecessary current will flow through this diode to the input and output, damaging the IC and equipment.
Products with an input tolerant function such as TC74VHC/VHCT, TC74LCX, TC74VCX (no input protective diode for forward direction from input to power supply) can apply an input signal even when power is not applied. Therefore, the loading sequence of (2) and (3) is not required.
The following documents also contain related information.