This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Start the control circuit first, followed by the other circuitry. Then, apply the control signals to place internal logic in a steady state and then apply other signals. The order is similar for bidirectional dual-power level shifters (buffer type) and unidirectional dual-power level shifters (buffer type).
Apply power supply and other signals in the following order. (Fig. 1)
#1. VCCA (power supply for circuit blocks with control circuits)
#2. VCCB (VCCA and VCCB may be powered up simultaneously.)
#3. Control signals (/OE, DIR)
#4. Input signals (A1 or B1)
The same order applies to the level shifter (bus switch type). (Fig. 2)
The following documents also contain related information.