This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Wired-OR logic in which multiple outputs are connected together is prohibited because they are short-circuited. Obviously, any output must not be connected to VCC or GND. (Fig. 1)
Multiple gates in the same package can be connected together as shown below to increase the drive capability.
However, it is recommended to use high-drive ICs instead, such as the 74AC, 74LCX and 74VCX series.
In order to improve the drive capability, the gates in the same package can be connected as shown in Fig. 2. However, it is recommended to use a IC with high drive capability such as 74AC, 74LCX, 74VCX Series.
The following documents also contain related information.