This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Each item (cut-off current, current gain, saturation voltage, transition frequency, collector output capacitance, noise figure) described in the electrical characteristics of the data sheet is explained. For the measurement methods of items 1 to 4, please refer to FAQ: Example of measurement of the key bipolar transistor characteristics.
Table. 1 shows an example of a data sheet description.
Depending on the product, there may be other electrical characteristics listed. The following application notes have explanations for other items. please refer.
The electrical characteristics and equivalent circuit:Bipolar Transistor Application Notes
See the application note below for details on absolute maximum ratings.
The maximum ratings:Bipolar Transistor Application Notes
The following documents also contain related information: