This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
This is a 2ch half-bridge (H-bridge) gate driver IC with the minimum functions required for automotive applications.
Compatible with body systems in general that use brushed motors.
In particular, by converting a system that uses mechanical relays to drive motors to semiconductors, high reliability and miniaturization can be achieved.
In recent years, there has been an increase in the demand for motors per vehicle due to the increasingly electrified moving parts of automotive equipment, which had been mechanical. The number of drivers driving motors is also increasing, and the system is becoming smaller and more integrated. Some motor applications require no rotational speed control, and a driver with limited functions and performance is required.
We are working to strengthen our product lineup to meet this demand, and TB9103FTG introduced here is part of this enhancement (Table 1).
Table 1. Lineup of Gate Driver IC for Automotive Brushed Motors
GD: Gate Driver, CP: Charge Pump, MCSA: Motor Current Sense Amplifier, SR: Safety Relay, Dev.: Development, xTBV: x Times Battery Voltage
| Part number | Status | Package | GD | CP | MC SA |
GD for SR |
SPI | Comment |
|---|---|---|---|---|---|---|---|---|
| TB9103FTG | MP | VQFN24 | ○ (H-bridge or 2ch Half-bridge) |
○ (2TBV) |
- | - | - | Propose to replace mechanical relay by semiconductor relay. |
| TB9104FTG | Dev. | VQFN32 | ○ (H-bridge or 2ch Half-bridge) |
○ (2TBV) |
○ (1ch) |
○ (1ch) |
○ |
Highly general purpose device with minimum functionality. |
| TB9052FNG | MP | HTSSOP48 | ○ (H-bridge) |
○ (3TBV) |
○ (1ch) |
- | - | Built-in motor control profile. |
| TB9057FG | MP | LQFP48 | ○ (H-bridge) |
○ (3TBV) |
○ (1ch) |
- | - | Operation under low battery voltage, Enhanced FuSa. Built-in Phase Monitor to monitor direction of motor operation. |
TB9103FTG is a gate-driver IC for controlling the external Nch-MOSFET that drives the brushed motors. In addition, various abnormal conditions (VDS, VGS, overtemperature, power supply, setting, etc.) are outputted at DIAG terminal. There are two DIAG jacks, which can be used to determine which channel of a half-bridge with two channels has an error.
TB9103FTG assumes that a microcomputer that enables high-level control is not used, but the through-current of external Nch-MOSFETs, which is the most important factor to avoid in a system, is avoided by the product's built-in automatic dead-time control.
The TB9103FTG has reduced the number of terminals by downsizing the functions, enabling the selection of a package that is among the smallest in the world. [Note 2]
Its dimensions are 16mm2 in 24pin of VQFN.
The QFN package is used to realize the small size of this product. Also, by hiding the corner pins that have GND potential in the mold resin, the risk of malfunctions due to short failures between pins is reduced.
Advantages of switching from mechanical relays to semiconductors (MOSFETs) include quiet operation (no relay noise), high reliability (long life), and small size (small mounting area).
The following figure (Figure 3) illustrates the image.
The power supply (VB, VCC) is intended for use with a 12V battery system. The guaranteed chip temperature range is -40℃ to 150℃, which corresponds to Grade1 in the AEC-Q100 [NOTE 3].
This product is equipped with a charge pump that can drive an external Nch-MOSFET. The main specifications are shown below (Table 2).
| Item | Symbol | Terminal | Limit Values | ||
|---|---|---|---|---|---|
| Min | Max | Unit | |||
| Power supply voltage operating range 1 | VCCrng | VCC | 4.5 | 5.5 | V |
| Power supply voltage operating range 2 | VBrng | VB | 7 | 18 | V |
Unless otherwise specified, VB=7 to 18V, VCC=4.5 to 5.5V (VB≧VCC) and Ta=-40 to 125℃.
| Item | Symbol | Terminal | Limit Values | |||
|---|---|---|---|---|---|---|
| Min | Typ. | Max | Unit | |||
| Charge pump voltage | VCP1 | VCP | VB+5 | VB+11 | VB+14 | V |
| Between the high-side GSs Drive voltage |
VGSHSSRC1 | GH1, GH2 | VCP-VB -0.2 |
- | VCP-VB | V |
| VGSHSSNK1 | GH1, GH2 | - | - | 0.5 | V | |
| Between the low-side GSs Drive voltage |
VGSLSSRC1 | GL1, GL2 | 8.9 | 11 | 14 | V |
| VGSLSSRC2 | GL1, GL2 | VB-0.1 | - | VB | V | |
| VGSLSSNK1 | GL1, GL2 | - | - | 0.5 | V | |
| Between the high-side GSs Drive output resistance Source direction |
Ronhssrc | GH1, GH2 | 250 | 500 | 1000 | Ω |
| Between the high-side GSs Drive output resistance Sink direction |
Ronhssnk | GH1, GH2 | 20 | 50 | 150 | Ω |
| Between the low-side GSs Drive output resistance Source direction |
Ronlssrc | GL1, GL2 | 250 | 500 | 1000 | Ω |
| Between the low-side GSs Drive output resistance Sink direction |
Ronlssnk | GL1, GL2 | 20 | 50 | 150 | Ω |
MODE setting:
Two types of mode selectable: H-bridge mode /Half-bridge mode
VDS Detect Level Setting:
This is the setting of the function to monitor abnormalities in the drain-source voltage of external Nch-MOSFETs.
The detection level can be set in 4 steps (disable function, 0.3V, 0.6V, 0.9V).
To enable customers to easily verify the characteristics of the TB9084FTG, we provide evaluation boards on free of charge. Of course, engineering samples can be submitted. Please contact our sales staff or our business partners at your service.
The size of the evaluation board is 95mm×75mm.
For customer convenience, switches, jumpers, and connectors are mounted as appropriate.
Toshiba is currently working to enhance a product lineup of ICs that control motors for automotive equipment. We will contribute to the electrification of automotive equipment and the improvement of comfort by introducing products to the market that optimize the functions and performance built into ICs to meet customers' needs.
[Note 1] Abbreviation for Electronic Control Unit, a device in which electronic components are mounted on a board.
[Note 2] According to our research in April 2022.
[Note 3] Reliability testing and other standards for automotive ICs defined by the Automotive Electronics Council.
Stock Check & Purchase
require 3 characters or more.
* Company names, product names, and service names may be trademarks of their respective companies.