This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Toshiba eFuse ICs are optimal products for short-circuit protection of USB terminal VBUS and power supply terminals. In addition, there are products that have obtained the IEC62368-1 standard, which can also contribute to obtaining IEC62368-1 certification for devices.
Regarding the short-circuit protection, the short-circuit condition is detected at high speed, and the output current is quickly limited by controlling the internal MOSFET.
It also incorporates overvoltage protection and slew rate adjustment functions, allowing the functions of other power supply ICs to be integrated into the Toshiba eFuse IC.
Specific usage methods are as follows. When using the TCKE8 series operates at voltages ranging from 4.5V to 18V. The overcurrent limit can be set to 0.5A ~5A using an external resistor.
Please refer to the link application notes and datasheets below for further details.
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.