This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Thermal shutdown is a function that switches off the internal output MOSFET to cut off the output current when a higher current continues to flow and the junction temperature of the eFuse IC exceeds the threshold.
Auto-retry type is that MOSFET turns on again when MOSFET shuts down and the junction temperature drops to the setpoint.
Latch type is that MOSFET is kept shut down after eFuse IC junction temperature has risen and TSD has been activated. Releasing the latch is performed by applying a reset by EN/ UVLO signal.
The figure below shows the operation image of the auto-retry type TSD function (TCKE8 series).
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.