※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
Knowledge
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
It is recommended to keep the capacitor connected to the output terminal below 500 pF.
If a large capacitor (capacitive load) is connected to the general-purpose logic IC, there is a possibility of malfunction due to the charge/discharge current that flows when the output mode transitions (H⇒L, L⇒H). It is recommended to keep the capacitor connected to the output pin to 500 pF or less, as there is a possibility that a current exceeding the specified value may flow through the output parasitic diode due to discharge. For loads higher than that, limit the discharge current via resistors as shown in Fig. 1 Please note that in this case, a delay occurs in the output signal.
Devices without an input-tolerant function such as the TC4000 and TC74HC/AC series should not also drive a large capacitive load because current could flow through the input protection diode if the power-off time is short.
It is recommended to keep the load capacitance connected to an input pin below 500 pF. If it is exceeded, insert a resistor as shown in Fig. 2 Note that there will also be a delay in the input signal in this case.
The following documents also contain related information.