This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
General-purpose logic IC is strong enough to withstand electrostatic discharge (EDS) standard. However, if static electricity of a greater intensity is applied to it, malfunction or damage may occur.
Because the oxide film at the input gate of a general-purpose logic IC is very thin (hundreds to thousands of angstroms), it could be damaged by an ESD of hundreds to thousands of volts.
To prevent ESD-induced damage, each input pin of Toshiba’s general-purpose logic ICs incorporates an ESD protection circuit. However, the internal ESD protection circuit has a limit.Therefore, inputs that might be exposed to excessive ESD (e.g., inputs connected to the external interface of a board) require ESD protection diodes to increase ESD protection capability. (Fig. 1)
The following documents also contain related information.