This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The I/O terminals that input signals do not need pull-up resistors, and the I/O terminals that output signals need to be pulled up to the power supply on the output side.
A dual power bus switch has the feature that the switch is turned off when the input signal of terminal A (or terminal B) exceeds the reference voltage based on VCCA.
This feature is used for voltage level shifting (level shifting).
Therefore, a pull-up resistor is not required on the input side of the signal, and it is necessary to pull up on the output side to the power supply on the output side.
When using in both directions (Fig. 1), a pull-up resistor (Rpullup-A, Rpullup-B) is required at both pins because both A and B sides may be output.
When using the input side and output side in one direction (Fig. 2), a pull-up resistor is not required at the input terminal (A side), but the output terminal (B side) must be pulled up (Rpullup-B) to the power VCCB at the output side.
When using in one direction in the reverse direction, a pull-up resistor is not required for the input pin (B side), but it is required to pull up (Rpullup-A) the output pin (A side) to the power VCCA of the output side.
The following documents also contain related information.