This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
A level shifter (voltage level translation IC) is an integrated circuit (IC) used to convert signal voltage levels between electronic circuits operating at different power supply voltages.
In signal transmission between systems with different voltage levels, communication may fail if the signal voltage levels are not compatible.
A level shifter is an IC that resolves this voltage gap.
In such transmission, the output voltage level must satisfy the input voltage level of the receiving system.
For example, if the output voltage level is too low to meet the input voltage level's VIH requirement, the signal cannot be transmitted (Figure 1).
Even in cases like this where the signal level is insufficient, using a voltage level translation IC (level shifter) makes it possible to bridge the voltage gap and enable signal transmission (Figure 2).
The following documents also contain related information.