This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Since there is no space to attach sensors to an ultra-small motor or sensors are too costly for an inexpensive motor, the rotor position is detected by the induced voltage.
The position is identified by the waveform of electromotive force (induced voltage) generated from the rotor rotation.
Only a square-wave drive can detect the rotor position by the induced voltage.
One set of coils among U phase, V phase, and W phase always has the current turned off. By detecting the point at which the amplitude of the motor drive waveform becomes 1/2 in its non-energized phase, the position of the rotor can be specified every 60 degrees.
The drawback of this approach occurs in the stop state. No position can be detected because no electromotive force is generated.