This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
For package information and/or land pattern examples for each product, please refer to the application note or webpage below.
(For reference) Package information can be searched in the Package & Packing Information>IC Packages web page.
Package & Packing Information>IC Packages
Example: The package name for TB67H480FNG is P-HTSSOP28-0510-0.65-001. Package information can be searched by applying full/part information of the package name to the package code column as shown below.
Search result will show the specific package information. Land pattern information will be shown as below.
Also package mounting guide can also be found on our website.
The following documents also contain related information.