This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The current transfer ratio (CTR) refers to the ratio of the collector current at the output side Ic to the input current passed to the LED at the input side IF expressed as a percentage. It is defined by the following formula.
CTR=(IC/IF)×100 (%)
As is the case with hFE for transistors, the current transfer ratio is an important parameter for transistor-output photocouplers. The value of this current transfer ratio has temperature Ta, LED current IF, and transistor collector-emitter voltage VCE dependencies. In addition, when an LED is energized for a long time, its optical output degrades gradually. Therefore, in designing, such deterioration over time must be taken into account.
Refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of Transistor Couplers", Chapter 1. Basic Characteristics.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)