This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
When input current IF reaches or exceeds a certain value, an IC coupler with amplifier circuit operates logically with its output being inverted. The threshold value for the input current required for inverting the output is called the "threshold input current" and is denoted by such symbols as IFHL and IFLH. This value varies depending on the product, and the maximum value for its variation is specified, for example, with IFHL(Max). In designing IF for actual use, also by considering LED deterioration over time, temperature, and design margin, a value larger than IFHL(Max) must be set for IF.
Also refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of IC Couplers", section 2.3.1.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)