This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Common-mode transient immunity is the maximum tolerable rate of rise (fall) of input/output common-mode voltage at which the specified High (Low) level can be maintained. A photocoupler has a small capacitance (0.6–0.8pF) between the input and output terminals. When an abrupt change in voltage occurs between the input and output terminals, a displacement current that occurs through this capacitance flows into the photodetector chip circuit, eventually causing malfunction. This phenomenon is likely to be felt more clearly in high-speed and high-sensitivity IC-output photocouplers, and thus calls for attention. As a method of preventing it, a shielding layer is provided on the surface of the photodetector chip to let noise signals flow to GND and prevent them from entering the photodetector circuit. This method applies to most of Toshiba IC coupler product groups.