This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Multi-bit TVS diodes are useful for sets with multiple-signal lines, such as USB or HDMI®. Packages employing the flow-through pin arrangement as described below can be easily mounted in a layout and can be efficiently patterned and wired. Especially, when high-speed signals are transmitted, differential signals are often used, and it is necessary to adjust the pattern width and length with a pair of (two) signal lines, and the flow-through type is also effective in such a case.
The above pattern is an example of a case where four signal lines are protected. DFN10 examples can be short-circuited between the left and right pins and can be mounted on the same line. DFN5 flow-through is achieved by staggering pins.
線上庫存查詢跟購買
型號需要超過三個文字以上
* The terms HDMI, and HDMI High-Definition Multimedia Interface, and the HDMI Logo are trademarks or registered trademarks of HDMI Licensing Administrator, Inc. in the United States and other countries.
* Other company names, product names, and service names may be trademarks of their respective companies.