Are there any constraints on the power-up sequence or the signal input order of dual power supply type voltage level translation ICs (level shifters)?

For dual power supply type voltage level translation ICs (level shifters), whether there are constraints on the power-up order and the signal input order depends on the product type.

■ Products without constraints
For 74AVC series, 74LVCxT series, there are no constraints on the power-up order of VCCA/VCCB or on the signal input timing. They can be used in any order.

■ Products with constraints
Other than the above, for buffer-type dual power supply level shifters / bus buffers (e.g., TC7SP3125 / TC7WP3125, TC7MP3125 / TC7MPN3125, TC74LCX163245 / TC74LCX164245 etc.), there are constraints on the power-up order and the signal input order.

Specifically, start the circuit block that contains the control circuit first, followed by the other power supply. Then, apply the control signals to place the internal logic in a steady state, and finally apply the input signals.

The order is the same for both the bidirectional dual power supply level shifter (buffer type) and the unidirectional dual power supply level shifter (buffer type). Using the bidirectional dual power supply level shifter (buffer type) as an example, apply power and signals in the following order (Fig. 1):

    #1. VCCA (power supply for circuit blocks with control circuits)
    #2. VCCB (VCCA and VCCB may be powered up simultaneously.)
    #3. Control signals (/OE, DIR)
    #4. Input signals (A1 or B1)

Fig. 1 Dual supply level shifter (Buffer type)
Fig. 1 Dual supply level shifter (Buffer type)

For details on the operation of the dual power supply bus switch type (TC7SPB / TC7WPB / TC7QPB / TC7MPB series, TC7MPB932x series, etc.), please refer to the following link.
Are there any constraints on the power-up/power-down sequence of a dual power supply bus switch?

Related Links

The following documents also contain related information.

FAQs

Product Lists

Application Notes

開啟新視窗