This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
General-purpose registers can be used for various purposes such as an accumulator and the data handling.
The TLCS-870/C1 has eight registers W, A, B, C, D, E, H and L (8 bit).
These eight registers can also be used as 16 bit registers by a pair of WA, BC, DE and HL.
These combinations are only for the registers next to each other, for example, B and E, H and E, etc. cannot be combined.
In addition, TLCS-870/C1 has two general-purpose registers IX and IY of 16 bit.
They are mainly used as an index registers when accessing the memory.
The TLCS-870/C1 has two banks of these registers.