This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Depending on the metal used, SBDs have a rated forward voltage (VF) between 0.4 V to 0.7 V, which is lower than the forward voltage of pn junction diodes. However, the withstand voltage of silicon SBDs is 20 to 150 V, not higher than that of pn junction diodes.
Toshiba also provides SBDs fabricated with a wide-bandgap semiconductor (SiC) having a high electric breakdown field that withstand up to 650 V.
Fig. 1 compares the band diagrams of pn junction diodes and SBDs in the non-biased state. The forward voltage (VF) of pn junction diodes is determined by a difference in potential energy between p-type and n-type semiconductors whereas the forward voltage (VF) of SBDs is determined by a difference between the work function of a metal and the electron affinity of an n-type semiconductor such as silicon (i.e., Schottky barrier). Therefore, SBDs with low VF can be created by using a metal that has a work function close to the electron affinity of the n-type semiconductor (e.g., silicon). Fig. 2 shows the difference in VF, depending on the metal used.
For products, please refer to the following links.