This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The LDO regulates its output voltage using negative feedback. The output voltage oscillates when the phase of the signal to detect changes in the output voltage (VOUT) lags by 180°, turning negative feedback into positive feedback. The LDO incorporates an error amplifier, a drive circuit for an output transistor, and the output transistor. The feedback loop has an inherent delay due to the capacitance and resistance of these circuits. If the loop has a gain, negative feedback turns into positive feedback when the phase delay due to this inherent delay reaches 180°, causing the difference between the output and reference voltages to be amplified.