This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Thermoflagger™ is an IC that can be used in conjunction with a PTC thermistor to detect abnormal heat output from an electronic device.
The resistance of a PTC thermistor is almost constant near room temperature. However, the resistance rises rapidly when the temperature increases and exceeds the detected temperature. Therefore, the thermistor is used to protect against overheating. Thermoflagger™ detects a resistive change in the PTC thermistor and inverts it if it overheats. Thermoflagger™ uses a circuit to detect resistive changes by constantly supplying a minute constant current to the PTC thermistor, allowing several PTC thermistors to be connected in series. As a result, it is possible to detect the temperature at any position in the electronic equipment. If you want to change the detected temp. at each position, it can be easily done by changing the PTC thermistor.
The following documents also contain related information.