This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
In recent years, MOSFETs have been used more often than bipolar-junction transistors (BJTs). This is because MOSFETs generally require no drive current and are easy to handle. However, BJTs are used in amplifiers, oscillators, switching at low voltages, etc.
This is because the BJT has higher gain (hFE)*, better linearity, better 1/f noise, and can be turned on by applying a voltage of about 0.7 V between the base and emitter. In addition, BJTs are sometimes used in environments with large disturbances due to their high resistance to static electricity (ESD).
An example circuit using BJTs is shown below.
*hFE varies with the collector-emitter voltage, which depends on external circuitry.
For a description of hFE, also see the FAQ entry, “What is the relationship between the base current and collector current of a bipolar junction transistor (BJT) ?”.
The following documents also contain related information: