This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
As a measure against EMI, it is possible to connect capacitors to the output lines of a motor driver IC.
EMI (Electromagnetic Interference) occurs when electromagnetic noise is emitted from electronic components such as semiconductors, causing malfunctions in external electronic parts or systems. Connecting capacitors to the output lines can help suppress the generation of electromagnetic noise.
One of the measures against EMI is shown in the Fig. 1. When a capacitor is connected to the output, an inrush current flows into the capacitor during switching. This inrush current is related to the capacity of the capacitor and the output slew rate of the IC.
Please select the capacity of the capacitor with a margin to ensure that the inrush current does not exceed the maximum rated current.
Please refer to the following example for selecting the capacity of the capacitor. Fig. 2 shows the output slew rate waveform of the stepping motor driver TB67S539FTG. The rise time [tr] is 65.0ns, and the fall time [tf] is 69.1ns.
・The inrush current [I] to the capacitor is estimated from the power supply voltage [Vm] and the capacitor’s impedance [ZC]
I=Vm/ZC……………………………………………………………(1)
・The impedance [ZC] of the output capacitor can be determined by the following formula from the slew rate [tr] and the capacitor capacity [C].
ZC =1/jωC ω=2π f=2π /tr…………………………………(2)
・Solving the above equation for [Imax], the maximum capacity [Cmax] of the output capacitor is as follow.
Cmax= Imax tr /2π Vm……………………………………………(3)
Here, the power supply voltage [Vm] is 24V, the maximum rated current [Imax] is 2A, and the slew rate [tr] is 65.0ns. From equation (3), the maximum capacity [Cmax] of the output capacitor can be calculated to be approximately 860pF. Please start testing with capacitors that have a capacity less than this value, allowing for a margin.
Please note that this calculation is only an example for reference and may differ from the actual situation depending on the characteristics of the components and the operating environment.
The following documents also contain related information.