This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The motor achieves maximum torque when the magnetic field of the magnet is behind the magnetic field of the coil by 90 degrees in phase. Since the induced voltage leads the magnetic field of the magnet by 90 degrees in phase, and the motor current is in phase with the magnetic field of the coil, maximum torque can be obtained when the phases of the induced voltage and the motor current are the same. Under this condition, the motor can be driven most efficiently.
However, as the figure below shows, when the drive voltage is applied in phase with the induced voltage, the phase of the motor current is delayed due to the coil’s inductive reactance. This results in a braking torque, consequently leading to lower efficiency.
To improve this, a correction method is employed that involves advancing the phase of the drive voltage, which in turn advances the phase of the motor current, aligning it with the induced voltage and thereby eliminating braking torque. This is known as the lead angle control, which can improve the efficiency of brushless DC motors.
The following documents also contain related information.