This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The absolute maximum ratings of a semiconductor device are a set of ratings that must not be exceeded, even for a moment.
Exceeding the rating(s) may cause the device breakdown, damage, or deterioration, and may result injury by explosion or combustion. Design so that the absolute maximum ratings are never exceeded under any operating conditions. The operating range is a specification to ensure normal IC operation, and it is essential to strictly adhere to this condition in practical use.
Example: Extract of TB6585AFTG’s data sheet,
The absolute maximum rating of power supply voltage is 45V. There will be a possibility of breakdown or damage to the IC when a voltage exceeding 45V is applied.
The operating range of power supply voltage is 4.5~42V. The IC can operate normally within this range. If the operating range is exceeded, there is a possibility that the IC will not function properly.
The following documents also contain related information.