This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
For transistor-output photocouplers, when LED current IF is passed to the input side, collector current IC flows at the output side. The transfer ratio of Ic to IF is called the current transfer ratio (CTR) and defined in the following formula:
CTR=(IC/IF)x100 (%)
As is the case with hFE for transistors, the current transfer ratio is an important parameter for transistor-output photocouplers.
Also refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of Transistor Couplers", section 1-1. Current Transfer Ratio.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)
For IC-output photocouplers, photorelays, and triac-output photocouplers, however, the threshold value current for input current IF reversing the output state for operation to be performed at the output side is defined as the threshold input current, and for photorelays and triac-output photocouplers, it is defined as the trigger LED current. When using any of the above photocouplers and phororelays, a value equal to or greater than the "threshold input current (max.)" or "trigger LED current (max.)" written in the data sheet must be set for the driving LED current setting.
Also refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of IC Couplers", section 2. 3. 1. Threshold input current IFLH, IFHL.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)