This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Vector control traditionally consumes much software resource. A microcontroller can not work effectively because of shortage of software resource if main capacity of the embedded memory is occupied by the vector control software. Toshiba has introduced a hardware IP into microcontrollers which handles complicated calculations in the vector control without detailed instructions by CPU. The hardware IP is Vector Engine. The Vector Engine performs transformation from 3-phase to 2-phase, rotation coordinate transformation, and those reverse transformations, which are main calculations in the vector control. The performance of the microcontrollers has been drastically improved when cooperating with the Vector Engine in vector controls.
Since the requirements for speed control and position estimation differ greatly among individual applications and users, they can be implemented via software. The vector engine provides great flexibility in allowing you to create various schedules that define a combined sequence of VE and user’s software operations to perform. The vector engine supports two operating modes: Scheduled mode that executes a series of operations consecutively and Single Task mode that executes individual tasks one by one. Schedules can select a task that causes the vector engine to start execution.
Microcontrollers products incorporating a Vector Engine are displayed.
線上庫存查詢跟購買
型號需要超過三個文字以上