This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The FLAG output is a function that notifies when the eFuse IC detects a specific fault.
Explanation of the TCKE9 Series Example.
Figure 1 shows the equivalent circuit of the FLAG terminal of the TCKE9 series. Since the FLAG terminal is an open-drain structure, it must be pulled up using an external resistor to an external supply.
When selecting the pull-up resistor, please fully consider the sink current (maximum rating) of the FLAG terminal and evaluate it sufficiently in the actual device. (As a reference, the pull-up resistor value is 10 kΩ.)
Table 1 shows the functions and timings of the FLAG output of the TCKE9 series. For details, please refer to the individual data sheets.
| Abnormal mode | FLAG power | Timing of FLAG Outputting Operation | IC operation |
|---|---|---|---|
| Superheating | Yes | Tj ≥ TSD 155 °C (Typ.) | Shutdown |
| Overvoltage | - | - | VOUT voltage-clamp |
| Low voltage | - | - | Shutdown |
| Overcurrent | - | - | IOUT Current Limit |
| Short-circuit | - | - | Shutdown |
| ILIM pin open | - | - | Shutdown |
| ILIM pin short-circuited | Yes | IOUT > 2 A (Typ.) | IOUT > 2A (Typ.) shutdown |
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.