This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The formats of output signals of remote controls depend on vendors, because they have not been standardized yet. Generally a long pulse called a leader is generated first when a button on a remote control is pushed, and the information of the button is following. Remote Control Signal Processor (RMC) detects the leader. Even when the leader is not existing, RMC detects another signal which a remote control generates instead.
A typical operation of RMC is as follows; In the case of an infrared remote control, the signal is transferred with infrared carrier to a receiver. After removing the carrier wave, the signal is transferred to RMC. Actually the signal has a lot of noises while the wave flies in the air between the remote control and the receiver. RMC sweeps the noises and recovers the leader signal. When it recognizes the leader, it generates an interrupt to CPU.
Microcontrollers products incorporating a Remote control signal processor are displayed.
線上庫存查詢跟購買
型號需要超過三個文字以上