This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The DIR pin determines the communication direction of the input/output pins, and the /OE pin controls whether the level shifter's output is enabled or disabled.
The “DIR pin” on bidirectional level shifters stands for Direction and determines the communication direction. Setting DIR to a high level enables communication from pin A to pin B, while setting it to a low level enables communication from pin B to pin A. This pin allows you to determine the signal communication direction.
The “/OE pin” stands for Output Enable and controls the on/off state of the output pins. The “/OE” pin with a slash (bar) enables communication at the L level and becomes an input impedance at the H level. The “OE” pin without a slash (bar) behaves in the opposite manner.
When multiple ICs are connected to the same signal line, a bus conflict (collision) may occur. In this case, controlling the output via the OE pin allows enabling the output only when necessary, while setting other ICs to Hi-Z prevents collisions.
Multiple outputs from a general-purpose CMOS logic IC come into conflict (Short-circuiting)
| Terminal | Explanation | State | Action |
|---|---|---|---|
| DIR | Determine the data communication direction | 1 (High) | A → B |
| 0 (Low) | B → A | ||
| /OE | Determine output ON/OFF | 0 (Low) | Output enabled (ON) |
| 1 (High) | Output disabled (OFF) |
The following documents also contain related information.