How does a high-voltage IPD detect temperature for thermal shutdown?

The thermal shutdown temperature is detected by monitoring the forward voltage (VF) of a temperature detection diode on a chip.

The forward voltage of the diode has a temperature coefficient of roughly -2 mV/°C. The forward voltage of the temperature detection diode is compared with the internal reference voltage, and when the forward voltage falls below the reference voltage because of an increase in temperature, the thermal shutdown threshold is tripped to protect the IPD from excessive temperature.

Fig. 1 Temperature detection circuit
Fig. 1 Temperature detection circuit
Fig. 2 V<sub>F</sub> voltage-Temperature
Fig. 2 VF voltage-Temperature

Related Links

The following documents also contain related information.

FAQs

Application Notes

開啟新視窗