This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
In general, The dual-power bus switch has no restrictions on the order in which the power is turned on and off. The device will not be damaged even if either power supply is turned on first. However, there may be restrictions on the power-on order, so please check the datasheet of each device for details.
The operation at power-up are described using TC7WPB9306FK as an example. (refer Fig. 1)
When VCCA is turned on and VCCB is turned on later, the switch does not turn on until about 1.5 V because the voltage enough to turn the switch on is not applied to the gate of the switch.
Also, if VCCB is on and VCCA is 0 V, the gate level converter will not start, so the switch will not turn on.
However, to use this device as a voltage level conversion IC (level shifter), please use at the condition (VCCA < VCCB).
The following documents also contain related information.